SysPropertiesThe constants defined in this class are initialized from system properties. Those properties can be set when starting the virtual machine:java -Dh2.baseDir=/tempThey can be set within the application, but this must be done before loading any classes of this database (before loading the JDBC driver): System.setProperty("h2.baseDir", "/temp"); ALIAS_COLUMN_NAMESystem property
h2.aliasColumnName .When enabled, aliased columns (as in SELECT ID AS I FROM TEST) return the alias (I in this case) in ResultSetMetaData.getColumnName() and 'null' in getTableName(). If disabled, the real column name (ID in this case) and table name is returned. This setting only affects the default mode. When using different modes, this feature is disabled for compatibility for all databases except MySQL. For MySQL, it is always enabled. In version 1.0, it is enabled by default. In version 1.1, it is disabled by default. ALLOWED_CLASSESSystem property
h2.allowedClasses (default: *).Comma separated list of class names or prefixes. ALLOW_BIG_DECIMAL_EXTENSIONSSystem property
h2.allowBigDecimalExtensions (default:
false).When enabled, classes that extend BigDecimal are supported in PreparedStatement.setBigDecimal. BIND_ADDRESSSystem property
h2.bindAddress (default: *).Comma separated list of class names or prefixes. CACHE_SIZE_DEFAULTSystem property
h2.cacheSizeDefault (default: 16384).The default cache size in KB. CACHE_SIZE_INDEX_SHIFTSystem property
h2.cacheSizeIndexShift (default: 3).How many time the cache size value is divided by two to get the index cache size. The index cache size is calculated like this: cacheSize >> cacheSizeIndexShift. CHECKSystem property
h2.check (default: true).Assertions in the database engine. CHECK2System property
h2.check2 (default: true).Additional assertions in the database engine. CLIENT_TRACE_DIRECTORYSystem property
h2.clientTraceDirectory (default:
trace.db/).Directory where the trace files of the JDBC client are stored (only for client / server). COLLATOR_CACHE_SIZESystem property
h2.collatorCacheSize (default: 10000).The cache size for collation keys (in elements). Used when a collator has been set for the database. DATASOURCE_TRACE_LEVELSystem property
h2.dataSourceTraceLevel (default: 1).The trace level of the data source implementation. Default is 1 for error. DEFAULT_LOCK_MODESystem property
h2.defaultLockMode (default: 3).The default value for the LOCK_MODE setting. DEFAULT_MAX_MEMORY_UNDOSystem property
h2.defaultMaxMemoryUndo (default: 50000).The default value for the MAX_MEMORY_UNDO setting. DEFAULT_MAX_OPERATION_MEMORYSystem property
h2.defaultMaxOperationMemory (default:
100000).The default for the setting MAX_OPERATION_MEMORY. DELAY_WRONG_PASSWORD_MAXSystem property
h2.delayWrongPasswordMax (default: 4000).The maximum delay in milliseconds before an exception is thrown for using the wrong user name or password. This slows down brute force attacks. The delay is reset after a successful login. The value 0 means there is no maximum delay. DELAY_WRONG_PASSWORD_MINSystem property
h2.delayWrongPasswordMin (default: 250).The minimum delay in milliseconds before an exception is thrown for using the wrong user name or password. This slows down brute force attacks. The delay is reset to this value after a successful login. Unsuccessful logins will double the time until DELAY_WRONG_PASSWORD_MAX. DOLLAR_QUOTINGSystem property
h2.dollarQuoting (default: true).Dollar quoting is used to quote text without having to use escape characters. A dollar quoted string starts and ends with $$. Inside the text, $$ is not allowed. EMERGENCY_SPACE_INITIALSystem property
h2.emergencySpaceInitial (default: 262144).Size of 'reserve' file to detect disk full problems early. EMERGENCY_SPACE_MINSystem property
h2.emergencySpaceMin (default: 65536).Minimum size of 'reserve' file. ENABLE_ANONYMOUS_SSLSystem property
h2.enableAnonymousSSL (default: true).When using SSL connection, the anonymous cipher suite SSL_DH_anon_WITH_RC4_128_MD5 should be enabled. FILE_ENCODINGSystem property
file.encoding (default: Cp1252).It is usually set by the system and is the default encoding used for the RunScript and CSV tool. FILE_SEPARATORSystem property
file.separator (default: /).It is usually set by the system, and used to build absolute file names. JAVA_SPECIFICATION_VERSIONSystem property
java.specification.version .It is set by the system. Examples: 1.4, 1.5, 1.6. LARGE_RESULT_BUFFER_SIZESystem property
h2.largeResultBufferSize (default: 4096).Buffer size for large result sets. Set this value to 0 to disable the buffer. LINE_SEPARATORSystem property
line.separator (default: \n).It is usually set by the system, and used by the script and trace tools. LOB_FILES_IN_DIRECTORIESSystem property
h2.lobFilesInDirectories .Store LOB files in subdirectories. In version 1.0, it is disabled by default. In version 1.1, it is enabled by default. LOB_FILES_PER_DIRECTORYSystem property
h2.lobFilesPerDirectory (default: 256).Maximum number of LOB files per directory. LOG_ALL_ERRORSSystem property
h2.logAllErrors (default: false).Write stack traces of any kind of error to a file. LOG_ALL_ERRORS_FILESystem property
h2.logAllErrorsFile (default:
h2errors.txt).File name to log errors. MAX_FILE_RETRYSystem property
h2.maxFileRetry (default: 16).Number of times to retry file delete and rename. MAX_MEMORY_ROWS_DISTINCTSystem property
h2.maxMemoryRowsDistinct (default:
Integer.MAX_VALUE).The maximum number of rows kept in-memory for SELECT DISTINCT queries. If more than this number of rows are in a result set, a temporary table is used. MAX_QUERY_TIMEOUTSystem property
h2.maxQueryTimeout (default: 0).The maximum timeout of a query. The default is 0, meaning no limit. MAX_RECONNECTSystem property
h2.maxReconnect (default: 3).The maximum number of tries to reconnect in a row. MAX_TRACE_DATA_LENGTHSystem property
h2.maxTraceDataLength (default: 65535).The maximum size of a LOB value that is written as data to the trace system. MIN_COLUMN_NAME_MAPSystem property
h2.minColumnNameMap (default: 3).The minimum number of columns where a hash table is created when result set methods with column name (instead of column index) parameter are called. MIN_WRITE_DELAYSystem property
h2.minWriteDelay (default: 5).The minimum write delay that causes commits to be delayed. OBJECT_CACHESystem property
h2.objectCache (default: true).Cache commonly used objects (integers, strings). OBJECT_CACHE_MAX_PER_ELEMENT_SIZESystem property
h2.objectCacheMaxPerElementSize (default:
4096).Maximum size of an object in the cache. OBJECT_CACHE_SIZESystem property
h2.objectCacheSize (default: 1024).Maximum size of an object in the cache. This value must be a power of 2. OLD_COMMAND_LINE_OPTIONSSystem property
h2.oldCommandLineOptions .Support old command line options. In version 1.0, it is enabled by default. In version 1.1, it is disabled by default. OPTIMIZE_DISTINCTSystem property
h2.optimizeDistinct (default: true).Improve the performance of simple DISTINCT queries if an index is available for the given column. The optimization is used if:
OPTIMIZE_DROP_DEPENDENCIESSystem property
h2.optimizeDropDependencies (default:
true).Improve the performance of DROP and DROP ALL OBJECTS by quicker scanning if other objects depend on this object. OPTIMIZE_EVALUATABLE_SUBQUERIESSystem property
h2.optimizeEvaluatableSubqueries (default:
true).Optimize subqueries that are not dependent on the outer query. OPTIMIZE_GROUP_SORTEDSystem property
h2.optimizeGroupSorted .Optimize GROUP BY queries if an index can be used that matches the group by columns. In version 1.0, it is disabled by default. In version 1.1, it is enabled by default. OPTIMIZE_INSystem property
h2.optimizeIn (default: true).Optimize IN(...) comparisons. OPTIMIZE_MIN_MAXSystem property
h2.optimizeMinMax (default: true).Optimize MIN and MAX aggregate functions. OPTIMIZE_NOTSystem property
h2.optimizeNot (default: true).Optimize NOT conditions by removing the NOT and inverting the condition. OPTIMIZE_SUBQUERY_CACHESystem property
h2.optimizeSubqueryCache (default: true).Cache subquery results. OPTIMIZE_TWO_EQUALSSystem property
h2.optimizeTwoEquals (default: true).Optimize expressions of the form A=B AND B=1. In this case, AND A=1 is added so an index on A can be used. OVERFLOW_EXCEPTIONSSystem property
h2.overflowExceptions (default: true).Throw an exception on integer overflows. RECOMPILE_ALWAYSSystem property
h2.recompileAlways (default: false).Always recompile prepared statements. REDO_BUFFER_SIZESystem property
h2.redoBufferSize (default: 262144).Size of the redo buffer (used at startup when recovering). RESERVE_MEMORYSystem property
h2.reserveMemory (default: 524288).This many bytes in main memory are allocated as a reserve. This reserve is freed up when if no memory is available, so that rolling back a large transaction is easier. REUSE_SPACE_AFTERSystem property
h2.reuseSpaceAfter (default: 16).Reuse space in database files after this many pages are free. REUSE_SPACE_QUICKLYSystem property
h2.reuseSpaceQuickly (default: true).Reuse space in database files quickly. SERVER_CACHED_OBJECTSSystem property
h2.serverCachedObjects (default: 64).TCP Server: number of cached objects per session. SERVER_RESULT_SET_FETCH_SIZESystem property
h2.serverResultSetFetchSize
(default: 100).The default result set fetch size when using the server mode. SHARE_LINKED_CONNECTIONSSystem property
h2.shareLinkedConnections .Linked connections should be shared, that means connections to the same database should be used for all linked tables that connect to the same database. In version 1.0, it is disabled by default. In version 1.1, it is enabled by default. SOCKET_CONNECT_TIMEOUTSystem property
h2.socketConnectTimeout (default: 2000).The timeout in milliseconds to connect to a server. SORT_NULLS_HIGHSystem property
h2.sortNullsHigh (default: false).Invert the default sorting behavior for NULL values, such that NULL values are sorted to the end of a result set in an ascending sort and to the beginning of a result set in a descending sort. TRACE_IOSystem property
h2.traceIO (default: false).Trace all I/O operations. USER_HOMESystem property
user.home (default: empty string).It is usually set by the system, and used as a replacement for ~ in file names. WEB_MAX_VALUE_LENGTHSystem property
h2.webMaxValueLength (default: 10000).The H2 Console will abbreviate result values larger than this size. lobCloseBetweenReadsSystem property
h2.lobCloseBetweenReads (default: false).Close LOB files between read operations. optimizeInJoinSystem property
h2.optimizeInJoin (default: false).Optimize IN(...) comparisons by converting them to inner joins. In version 1.0, it is disabled by default. In version 1.1, it is enabled by default. runFinalizeSystem property
h2.runFinalize (default: true).Run finalizers to detect unclosed connections. scriptDirectorySystem property
h2.scriptDirectory (default: empty
string).Relative or absolute directory where the script files are stored to or read from. |